Technical FAQs

Ask a Question

What are the different File Formats for Symate Plus?

Goals and Symptoms

What are the different File Formats for Symate Plus?

Causes and Fixes

There are 3 different File Formats for Symate Plus. They are:
SP2 = Symate Plus version 2
SP1 = Symate Plus version 1
SFW = Symate SFW3XX

The SFW that you have and the version of the software will determine what File Formats are available.

SFW 472 Symate Plus, Version 2 only, contains the option of selecting all 3 File Formats, SP1, SP2 and SFW. With this you can take programs and go between the different versions of software changing the file format to work in any version of software.

The formats are as follows:
 

File Format
text text
File Extension
text text
SP2
.RNG
.REG
.LAB
.HDR
.TTL
SP1
.PRG
.LAB
.HDR
.TTL
text
SFW
.RNG
.REG
.LBL
text text
.RNG = Rungs .LAB = Labels .TTL = Title
.REG = Registers .LBL = Labels
.PRG = Program .HDR = Headers

Legacy KB System (APS) Data: RESL1400 V3.0, Originally authored by RiTa on 05/01/2012, Last Edited by BrWa on 05/01/2012
Related ranges: SY/MATE
Was this helpful?
What can we do to improve the information ?