Technical FAQs

Ask a Question

When exporting an NxT database as a .DIF file, what do the four different listings mean?

When you export a ProWorx NxT database as an Excel Spreadsheet .DIF file, you will notice that
there are four different listings for the same address. The four listings reference a different section
of your documentation. The following codes in Column B of the Excel Spreadsheet can be translated as:
 

Column B Code Translation From NxT Documentation Editor
D Descriptor information
S Short Comment information
L Long Comment number
T Page Title information

Legacy KB System (APS) Data: RESL1318 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?