Technical FAQs

Ask a Question

Using the ExecLoader what does the 'Node #- Illegal Modbus function call' error message mean'?

This ExecLoader is packaged and used with Proworx Nxt as well as Concept. This error can occur when the PLC that is being addressed is not supported by Concept.


Legacy KB System (APS) Data: RESL1224 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?