Technical FAQs

Ask a Question

Why can I communicate to my 584A and 584M controller with my P190 and can't with ProWORX NxT?


The ProWORX NxT software will only communicate with the Level 3 or Level 4, 584 controllers. Any 584 A or 584M that part number starts with a -1XX is a level 1 or a level 2 controller. E.g. AS-584A-110 or AS-584M-110. These will not work with the ProWORX NxT software and you will need to continue to use your P190.

text
584A
584M
584L
ProWORX
NO
NO
YES
P190
YES
YES
YES

NOTE: The 584 and Proworx software sofware have been obsoleted for years and upgrades are available by contacting your local distributor or contacting customer.services@schneider-electric.com for more informaiton.
Was this helpful?
What can we do to improve the information ?