Technical FAQs

Ask a Question

What memory cartridges can I use with my Twido?

Goals and Symptoms

What memory cartridges can I use with my Twido?

Causes and Fixes

There are two optional memory cartridges available, the 32 KB (TWDXCPMFK32, for backup only), and the 64 KB (TWDXCPMFK64). The memory cartridges provide additional memory for application storage.
The memory cartridges are used to:
 

  • Provide a removable backup of the application.
  • Load an application into a controller if certain conditions exist.( i.e. no battery backup)

The following table presents the available memory cartridge for each controller.
Memory Cartridge
Compact 10 I/O
Compact 16 I/O
Compact 24 I/O
Modular 20 I/O
Modular 40 I/O
TWDXCPMFK32
yes
yes
yes
yes
yes
TWDXCPMFK64
no
no
no
yes
yes
The TWDXCPMFK32 memory cartridge is for back up only. The TWDXCPMFK64 memory cartridge is for back up and expansion.

Legacy KB System (APS) Data: RESL122041 V4.0, Originally authored by JaBo on 12/02/2008, Last Edited by BrWa on 06/08/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?