Technical FAQs

Ask a Question

Where can the DFB used with the Momentum 170AEC92000 module be found in Concept v2.5 or greater?


The AEC DFB is located in the Concept/Dat folder with the name AEC.ASC. The file must be imported into Concept by following the procedure detailed below:

1. Move the file AEC.ASC to the Concept/DFB folder.
2. Open the Concept Converter utility.
3. Select FILE.
4. Select IMPORT.
5. Select the file AEC.ASC.
6. Hit "OK".
7. After successful completion of the import, the AEC DFB will be added to the DFB library, making it available for use in logic.


Legacy KB System (APS) Data: RESL122019 V3.0, Originally authored by MiMa on 02/27/2013, Last Edited by DaSo on 02/27/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?