Technical FAQs

Ask a Question

How do you create a help file for a Concept custom DFB?

Use the Concept DFB Editor to open the custom DFB. From the Menu choose <Project> < Properties>. Enter the help information in the 'Description:' box. Save and close the DFB. Insert the DFB in a project. Click on 'Help on Type'. The help information will be displayed.


Legacy KB System (APS) Data: RESL121853 V2.0, Originally authored by RiVe on 10/28/2008, Last Edited by DaSo on 10/28/2008
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?