Technical FAQs

Ask a Question

Can an M1E with a Modbus Plus option adapter be used as a bridge from Ethernet to Modbus Plus?


No, an M1E with a Modbus Plus option adapter installed cannot be used as a bridge from Ethernet to Modbus Plus.


Legacy KB System (APS) Data: RESL121801 V2.0, Originally authored by MiMa on 06/06/2013, Last Edited by DaSo on 06/06/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?