Technical FAQs

Ask a Question

What is the maximum number of configurable variables for the Twido controllers?


The maximum number of configurable variables for each Twido controller is detailed in the table below:

 

Item
Compact Base Controllers
text text
Modular Base Controllers
text text text text
text
10DRF
16DRF
24DRF
20DUK
20DTK
20DRT
40DUK
40DTK
Timers
64
64
128
128
128
128
128
128
Constants
64
64
64
64
64
64
64
64
Counters
32
32
32
32
32
32
32
32
Fast counters
3
3
3
2
2
2
2
2
Very fast counters
1
1
1
2
2
2
2
2
LIFO/FIFO registers
4
4
4
4
4
4
4
4
Schedule blocks
16
16
16
16
16
16
16
16
Drum controllers
4
4
8
8
8
8
8
8
PLS/PWM
0
0
0
2
2
2
2
2
Step counter
8
8
8
8
8
8
8
8
Shift bit register
8
8
8
8
8
8
8
8

Legacy KB System (APS) Data: RESL121711 V2.0, Originally authored by MiMa on 06/08/2012, Last Edited by BrWa on 06/08/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?