Technical FAQs

Ask a Question

Can a keyboard or mouse be connected to the mini-din connector on the front of the Magelis IPC without rebooting the unit?


Yes the IPC will recognize a device that has been plugged in hot.


Legacy KB System (APS) Data: RESL121544 V2.0, Originally authored by on , Last Edited by on
Related ranges: Magelis Modular iPC
Was this helpful?
What can we do to improve the information ?