Technical FAQs

Ask a Question

Can an external monitor be connected to the Magelis IPC?


Yes an external monitor can be connected via the VGA port on the control box.
The external monitor will have the identical display as the front panel attached to the control box.


Legacy KB System (APS) Data: RESL121542 V2.0, Originally authored by on , Last Edited by on
Related ranges: Magelis Modular iPC
Was this helpful?
What can we do to improve the information ?