Technical FAQs

Ask a Question

How are local variables created with Monitor Pro 7.0 Client Builder?


Local variables are created with Monitor Pro 7.0 by adding the percent " % " character to the end of the
variable name.

For example: MyVariableName%

A local variable, MyVariableName, will be created and reside on the client.


Legacy KB System (APS) Data: RESL121026 V2.0, Originally authored by MiMa on 09/28/2012, Last Edited by GeMc on 09/28/2012
Related ranges: MPRO CLIENT SERVER
Was this helpful?
What can we do to improve the information ?