Technical FAQs

Ask a Question

How can a floating point value be moved into 4XXXX registers in a Quantum PLC with 984 LL?


A floating point value can be moved into 4XXXX registers with the equation network. An example of moving a floating point value of 123.456 into registers 40001 and 40002 is shown below:

 
Was this helpful?
What can we do to improve the information ?