Technical FAQs

Ask a Question

What is the maximum number of web client connections that may be attached to a Monitor Pro 2.1 server?


The maximum number of web client connections that may be attached to a single Monitor Pro 2.1 server is 50.


Legacy KB System (APS) Data: RESL120808 V1.0, Originally authored by on , Last Edited by on
Related ranges: Monitor Pro
Was this helpful?
What can we do to improve the information ?