Technical FAQs

Ask a Question

What communication protocols are supported by the Twido PLCs?

ASCII (American Standard Code for Information Interchange) and Modbus are the only two supported protocols.

Legacy KB System (APS) Data: RESL120585 V2.0, Originally authored by RiTa on 05/02/2013, Last Edited by GeMc on 05/02/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?