Technical FAQs

Ask a Question

Does the Twido PLC have an integrated RTC ( Real Time Clock) function?

No, they do not have integrated real time clock function. In order to utilize the RTC function, it is necessary to use the optional plug-in RTC module. The part number for the RTC module is TWDXCPRTC.

Legacy KB System (APS) Data: RESL120584 V2.0, Originally authored by RiTa on 07/19/2013, Last Edited by GeMc on 07/19/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?