Technical FAQs

Ask a Question

Why are all three outputs of my 984 Ladder Logic Xmit constantly on?

All three outputs of the Xmit block will turn on to indicate the Xmit loadables were installed in the incorrect order. The NSUP loadable needs to be installed into the database first followed by the Xmit loadable.


Legacy KB System (APS) Data: RESL120573 V2.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?