Technical FAQs

Ask a Question

Why are only three of the five descriptor lines displayed on Proworx when I do a printout?


The number of descriptor lines displayed is configured in the Database Setup. The default value for the Number Network Listing Fields is set to three, limiting the number of descriptor lines printed to three. Increase the value to five. This will allow five descriptors to be displayed in the print out of the database.


Legacy KB System (APS) Data: RESL120522 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?