Technical FAQs

Ask a Question

Can I splice the cabling in the RIO network?

No. The cable cannot be spliced. However, you can install a tap (P/N MA-0185-100) onto the trunk cable and terminate the unused drop port with a Tap Port Terminator (P/N 52-0402-000). Remember that the tap has a 0.8 dB insertion loss in the RIO signal.

Was this helpful?
What can we do to improve the information ?