Technical FAQs

Ask a Question

Can third party communication protocols be purchsed for the XBTL1000 software?


Yes, third party communication protocols are available as separately purchased items. The protocols
are distributed on CD ROM, part number XBTL1PROT.
The protocols included on the CD are: Allen-Bradley DF1 & DH485 , GE Fanuc SNPX , Omron Sysmacway , and
Seimens AS511, 3964R , PPI and MPI.


Legacy KB System (APS) Data: RESL120421 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-F, TXBT-F
Was this helpful?
What can we do to improve the information ?