Technical FAQs

Ask a Question

What does the OURBUS error indicate on my Remote I/O Interface module?

The OURBUS error is an indication of a mismatch between the I/O modules in the rack and the I/O map (Traffic cop) configuration.
First, check the interface module (J89x/ P89x) for the proper address settings.
Then view the I/O map (Traffic cop) for that particular drop.
The modules entered in the I/O map (Traffic cop) must match those physically in the rack.
Each module must have a green Active light.
Any modules that are missing from the rack or do not have "Active" lights will produce an OURBUS error on the interface module.

Was this helpful?
What can we do to improve the information ?