Technical FAQs

Ask a Question

What is the minimum cable distance between MB+ taps?

For the Modbus Plus taps the minimum distance between nodes is ten feet. (10ft)
The length of the drop cable from the tap is included in the distance specification.
Therefore the formula is: (one drop length + second drop length + distance between taps => 10 ft )
If the drops cables are 10 ft. long , there is no minimum distance between taps.

Was this helpful?
What can we do to improve the information ?