Technical FAQs

Ask a Question

Why does Concept use 100% of the CPU capacity when there are no projects open?

This is an architectural decision made by the product development team. In the Concept kernel an idle task is running to consume all time slices. This allows Concept to poll the communication layers for requests, even if there is no connection established or no project opened. This task runs with the lowest priority. Therefore, if any other task is called, Concept does not prevent the task from executing.

Was this helpful?
What can we do to improve the information ?