Technical FAQs

Ask a Question

Can I use floating point format with multiple pens in XBTL1000 ?

Yes.....When using multiple pens the registers are assigned consecutively and when foating point format is used it automatically allows for IEEE format.


Legacy KB System (APS) Data: RESL115 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-L
Was this helpful?
What can we do to improve the information ?