Technical FAQs

Ask a Question

Can there be more then one version of Concept installed on a PC when using the FactoryCast utility?


It is not recommend that you have more than one version of Concept installed on your PC if you are using the FactoryCast utility. If you have multiple versions installed, linking the variable look up list from Concept into FactoryCast may be impacted. Refer to the readme file in FactoryCast 2.2.1 and later section 3.4, Using FactoryCast with Concept 2.5 XL.

Was this helpful?
What can we do to improve the information ?