Technical FAQs

Ask a Question

What is the purpose of the "Delay" parameter on the Modbus port of a Modicon PLC?


The "Delay" parameter on the Modbus port of a Modicon PLC is a time delay value from 10 milliseconds to 1 second. The value entered sets the amount of time the Modicon PLC waits after receiving a Modbus message before sending an acknowledgment.


Legacy KB System (APS) Data: RESL1142 V2.0, Originally authored by MiMa on 03/17/2012, Last Edited by MiOB on 03/17/2012
Related ranges: Modbus
Was this helpful?
What can we do to improve the information ?