Technical FAQs

Ask a Question

Why does the DIO head disappear when the Proworx 32 traffic cop is closed and reopened?

The DIO entry will disappear from the Traffic Cop tree if the drops in the DIO head are empty. To correct this issue, add an I/O module to one of the DIO drops.


Legacy KB System (APS) Data: RESL1033 V2.0, Originally authored by MiMa on 02/26/2013, Last Edited by DaSo on 02/26/2013
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?