Technical FAQs

Ask a Question

Can both incremental and absolute encoders be used on the same 170AEC92000 Momentum high speed counter base?

No, both incremental and absolute encoders cannot be used on the same 170AEC92000 Momentum high speed counter base. The counter ASIC will not support mixed operation with both incremental and absolute encoders.


Legacy KB System (APS) Data: RESL1016 V2.0, Originally authored by MiMa on 03/01/2013, Last Edited by DaSo on 03/01/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?