Technical FAQs

Ask a Question

What is the analog inputs range in voltage mode ?

In IMC hardware guide, 04/2012 (s1a10252.06.pdf) and in IMC Instruction Sheet (bbv60941_02.pdf), a schematic shows that analog inputs AI51 and AI52 range in voltage mode is 0-10 V.
These inputs only support 0-5 V.

Correction will be applied in the next release of thesee documents.
Was this helpful?
What can we do to improve the information ?