Technical FAQs

Ask a Question

How to use the SysTimeRtcSet function ?

In order to update the plc RTC , we recommand to use the SysTimeRtcSet function as below :
-> call this function in a CYCLIC task
-> manage a rising edge to set up the RTC (see example below)
-> do NOT set up the RTC every few milliseconds but every minute, every hour



Legacy KB System (APS) Data: RESL206839 V1.0, Originally authored by AnVi on 12/06/2011, Last Edited by AnVi on 12/06/2011
Related ranges: SoMachine, Modicon M258
Was this helpful?
What can we do to improve the information ?