Technical FAQs

Ask a Question

How to link variables from Unity Pro to Vijeo-Designer?

Steps to repeat:
- in Unity Pro, export variables in *.XVM format file, for example "export.XVM". This file can be saved on any driver (hard disk drive, USB memory stick...)

- in Vijeo-Designer, from Variables menu, use "Link Variables" command. Then select the correct file type: "UnityPro symbol export files (*.XVM)". Finally, choose the "export.XVM" file.

IMPORTANT: Please note that the*.STU format files can be used with "link Variables" command ONLY when Unity Pro XL is installed on the same PC where Vijeo-Designer is installed.


Was this helpful?
What can we do to improve the information ?