Technical FAQs

Ask a Question

During Unity Pro V2.3 installation, the following error message is displayed: "error 1904. Module C:\WINDOWS\system32\SKCL.dll failed to register. HR...

Goals and Symptoms

During Unity Pro installation, the following error message is displayed:
"error 1904. Module C:\WINDOWS\system32\SKCL.dll failed to register. HRESULT -2147023898. Contact your support personel".

Causes and Fixes

This issue can occur on some specific PC configurations.

- It is the SKCL.dll file which is not registered.
- If the install did not properly install the file c:/windows/system32/skcl.dll then this error can occur.
- To fix this issue, register the file as described below:
Find the ../system32/skcl.dll file and register it by dragging and dropping it on to the file c:/windows/system32/regsrvr32.exe
- Make sure that all updates for the Microsoft Operating System are applied.
- This can also occur if a virus protection software is running such as, Cylance Protect.
 


Legacy KB System (APS) Data: RESL179802 V2.0, Originally authored by LaBa on 03/08/2007, Last Edited by LaBa on 03/08/2007
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?