Technical FAQs

Ask a Question

What could cause a "OL9-1509 Controller is already logged in to another programming panel" error in Concept?

The most common cause of this error is when on-line to the PLC via Ethernet and the PC crashes or communication is lost because of network problems. To try to resolve this error, pull the Ethernet cable out of the 140NOE771xx and put it back in so that the module goes through a reset. This should clear the error when going back on-line with Concept.


Legacy KB System (APS) Data: RESL212563 V1.0, Originally authored by RoAl on 09/23/2013, Last Edited by RoAl on 09/23/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?