Technical FAQs

Ask a Question

Is there a document that explains how to design a control network for the M340 PAC?

Yes, attached below is a TVDA guide that presents the design and implementation of several PAC-to-PAC communications network models based on the Premium and M340 PAC families. All of the models described in this TDVA feature an Industrial Ethernet backbone. Industrial Ethernet is a switched based, full duplex network technology that offers scalability, low cost, reliability and deterministic message arrival times. Industrial Ethernet also supports highly reliable ring network designs.
TVDA-How-To-Design-a-Control-Network-Part1.zip


Legacy KB System (APS) Data: RESL212547 V1.0, Originally authored by BrWa on 09/20/2013, Last Edited by BrWa on 09/20/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?