Technical FAQs

Ask a Question

Where are the Quantum CPU Ethernet port IO Scanner health bits in Unity Pro?

The health bits for the IO Scanner service on the Quantum built-in CPU ethernet port are located at %SW160 - %SW167


Was this helpful?
What can we do to improve the information ?