Technical FAQs

Ask a Question

Can a 984 support Quantum I/O?

Only the PC-E984-785 supports Quantum I/O. This is accomplished via Remote I/O. The PC-E984-785 must be upgraded with the AM-E785-QKO upgrade kit. With this kit. the 785E can support up to 16 drops total of 800 series I/O and Quantum I/O. Each drop must be either 800 series or Quantum series. Mixing of types within a drop is not supported. The AM-E785-QKO kit contains the following:
A special 785E executive firmware p/n SW-E785-Q00
A special S908 module (RI/O head) executive cartridge p/n AS-Q908-016

Legacy KB System (APS) Data: RESL212300 V1.0, Originally authored by RoAl on 08/14/2013, Last Edited by RoAl on 08/14/2013
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?