Technical FAQs

Ask a Question

When printing a WebGate session, why is the frame blacked out?

Unfortunately inside the frame is "dynamic" per the Active X control. Internet Explorer cannot capture this dynamic content when spooling to the printer. A simple work around not being able to print, is to take a screen shot, and print from your image editor.


Legacy KB System (APS) Data: RESL212272 V1.0, Originally authored by GeMc on 08/08/2013, Last Edited by GeMc on 08/08/2013
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?