Technical FAQs

Ask a Question

Is there an adapter plate required to upgrade a Magelis XBTGT5230 to a HMIGTO5310?

Yes, the cutout dimension on the XBTGT5230 and HMIGTO5310 are different. The HMIGTO5310 would required an adapter XBTZGCO4 to fix in the same cutout.

Legacy KB System (APS) Data: RESL211911 V1.0, Originally authored by GeMc on 06/27/2013, Last Edited by GeMc on 06/27/2013
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?