Technical FAQs

Ask a Question

Does the TSX Compact 984 have a model with a "Built-in" Ethernet Port?

No, the TSX Compact 984 does not have a model with a "Built-in" Ethernet Port. One of our Schneider Electric Alliance partners, Niobrara R&D Corporation, does offer the CNOE-311 which is an Ethernet option module for the TSX Compact 984 Model PCE984258/265/275/285. Here's the URL for more information on the CNOE-311 -

NOTE: As of 2015 the Compact line has been obsoleted and the recommended replacement for this is the M340, for questions on this upgrad option contact tech support 888-266-8705.
Legacy KB System (APS) Data: RESL211590 V1.0, Originally authored by BrWa on 05/28/2013, Last Edited by BrWa on 05/28/2013
Related ranges: Legacy PB
Was this helpful?
What can we do to improve the information ?