Technical FAQs

Ask a Question

What TCP ports does Unity Pro use when connected to a M340 via ModbusTCP?

Unity when connecting via ModbusTCP to a PLC will request a programming connection to the remote PLC's ModbusTCP server port 502. Since it is a TCP connection, Unity will use a Client TCP port that is greater than 1024.


Was this helpful?
What can we do to improve the information ?