Technical FAQs

Ask a Question

What are the replacements for a TSXETY110 and a TSXETY110WS Premium Ethernet modules?

The replacement for a TSXETY110 is a TSXETY4103. The replacement for a TSXETY110WS ( with web server) is a TSXETY5103. The replacements are identical in functionality to the obsolete modules they replace respectively. While the IP addresses of TSXETY110/110WS were set using rotary switches, they are set using the software in the TSXETY4103 and TSXETY5103 modules.


Legacy KB System (APS) Data: RESL210028 V1.0, Originally authored by TVe on 12/14/2012, Last Edited by TVe on 12/14/2012
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?