Technical FAQs

Ask a Question

What is the highest Modbus RTU register offset that can be used in a Quantum processor?

The highest Modbus RTU register offset address that can be usedis 4 + 65535. The offset of a Modbus slave data area definition is 16 bits, therefore the highest address is FFFF Hex or 65,535 Decimal. The valid address offsets for Modbus are:
400001 - 465535
300001 - 365535
100001 - 165535
000001 - 065535


Legacy KB System (APS) Data: RESL209673 V1.0, Originally authored by BrWa on 11/15/2012, Last Edited by BrWa on 11/15/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?