Technical FAQs

Ask a Question

Download application using USB stick on XBTSTU655

Goals and Symptoms

On HMISTU655 PV:02, RL:01 SV:1.0, it is impossible to download application using USB Stick memory.

Causes and Fixes

We have published an IQ 102392 and recall the stock to update it in the manufacture plan. This new version PV:02, RL:02 SV:2.0 require to use a new software version. It is mandatory todownload the VJD5.1 SP1 and VJDSP1Hotfix1 from Schneider Live Update or Planet and install them on the PC


Legacy KB System (APS) Data: RESL202641 V1.0, Originally authored by JaOu on 06/29/2010, Last Edited by JaOu on 06/29/2010
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?