Technical FAQs

Ask a Question

What is the replacement for the TSXSUPA02 ASI power supply?


The TSXSUPA02 (2.4 A @ 30VDC) is replaced by either the ASIABLB3002 (2.4 A@ 30VDC ) or ASIABLD3002 (2.4 A @ 30VDC with ground fault detection) ASI power supplies.
 


Legacy KB System (APS) Data: RESL199663 V1.0, Originally authored by GeMc on 08/20/2009, Last Edited by GeMc on 08/20/2009
Related ranges: AS-Interface, Other PLCs
Was this helpful?
What can we do to improve the information ?