Technical FAQs

Ask a Question

What is the cable needed to connect the M340 to the XBTGT 2xxx terminals?

The cable combination that is needed is the XBTZ938 + XBTZG909.
It will connect the M340 and the following terminals:
XBTGT2110
XBTGT2120
XBTGT2130
XBTGT2220
XBTGT2330
XBTGT4230
XBTGT4330
XBTGT4340
XBTGT5230
XBTGT5330
XBTGT5340
XBTGT6330
XBTGT6340
XBTGT7340.


Legacy KB System (APS) Data: RESL188745 V1.0, Originally authored by GeMc on 10/30/2007, Last Edited by GeMc on 10/30/2007
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?