Technical FAQs

Ask a Question

What is a ConneXium USB memory backup adapter module ( TCSEAM0100)?

Goals and Symptoms

What is a ConneXium USB memory backup adapter module ( TCSEAM0100)?

Causes and Fixes






The TCSEAM0100 USB memory backup adapter is a device for storing and updating configuration data and software of a TCSESM switch.

In the case of a switch failure, the EAM enables a very simple configuration data transfer by means of a substitute switch of the same type.

Was this helpful?
What can we do to improve the information ?