Technical FAQs

Ask a Question

What is the current draw for the Quantum Unity Processor's 140CPU65XX0?

The power consumption of the Quantum Unity CPU'S:
140CPU65150 2,16A
140CPU65160 2,76A
140CPU67160 2,5A
The correct values are given by Power and IO calculator in Unity V2.0.2.

Note: These values do not include the PCMCIA consumption.


Was this helpful?
What can we do to improve the information ?