Technical FAQs

Ask a Question

Where can I download the Modbus Plus MBX Driver Suite?

This driver is not free. The MBX Driver Suite can be purchased thru your local Schneider Electric
dealer. The part number for the MBX Modbus Plus Driver Suite is SWMXDS001 for a single copy
license. Please contact your distributor for multi-user licenses.

Legacy KB System (APS) Data: RESL181314 V1.0, Originally authored by GeMc on 12/30/2006, Last Edited by GeMc on 12/30/2006
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?