Technical FAQs

Ask a Question

What are the cables needed to connect the XBTGT terminals to the Premium, Micro and Twido PLCs?

The following table lists the cables that can be used with the Premium, TSX Micro, TSX Nano and
Twido PLCs that have the round mini DIN connector.
 

Cable Part Numbers
Terminals
XBTZ968 (2.5 m)
XBTZ9680 (2.5 m right angle)
XBTZ9681 (5 m)
XBTZ9686 (16 m)
XBTZ9687 (20 m)
XBTZ9688 (25 m)

You also need to use this adaptor
with the above cables - XBTXG909
XBTGT2110
XBTGT2120
XBTGT2130
XBTGT2220
XBTGT2330
XBTGT4230
XBTGT4330
XBTGT4340
XBTGT5230
XBTGT5330
XBTGT5340
XBTGT6330
XBTGT6340
XBTGT7340

Legacy KB System (APS) Data: RESL181312 V1.0, Originally authored by GeMc on 12/30/2006, Last Edited by GeMc on 12/30/2006
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?