Technical FAQs

Ask a Question

Why is ProWORX Nxt reporting that I am missing the Andale Mono Linetype font?


The Andale Mono Linedraw font is necessary for Proworx Nxt to display and print logic.

1. Unzip the font.
2. Copy the font to the FONTS directory located in either the WINNT or System or System32 folders of the operating system.


andalemonolinedraw.zip


Legacy KB System (APS) Data: RESL181308 V1.0, Originally authored by GeMc on 12/30/2006, Last Edited by GeMc on 12/30/2006
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?